0613IB1313-10

Circuit Breaker Control Commands

Open Circuit Breaker

To open the circuit breaker, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E/P/H

Description

0x1F3F

8000

INT16U

904

A/E/P/H

Command code = 904

0x1F40

8001

INT16U

10

A/E/P/H

Number of parameters (bytes) = 10

0x1F41

8002

INT16U

4609

A/E/P/H

Destination = 4609 (0x1201)

0x1F42

8003

INT16U

1

A/E/P/H

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

A/E/P/H

Password of the command: Administrator or Operator user profile password

Close Circuit Breaker

To close the circuit breaker, the user must set up the command registers the following way:

Address

Register

X

Unit

Type

Range

A/E/P/H

Description

0x1F3F

8000

INT16U

905

A/E/P/H

Command code = 905

0x1F40

8001

INT16U

10

A/E/P/H

Number of parameters (bytes) = 10

0x1F41

8002

INT16U

4609

A/E/P/H

Destination = 4609 (0x1201)

0x1F42

8003

INT16U

1

A/E/P/H

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

A/E/P/H

Password of the command: Administrator or Operator user profile password

Enable/Inhibit a Circuit Breaker Close Order

To enable or inhibit a close order of the circuit breaker, the user must set up the command register the following way:

Address

Register

X

Unit

Type

Range

A/E/P/H

Description

0x1F3F

8000

INT16U

910

A/E/P/H

Command code = 910

0x1F40

8001

INT16U

13

A/E/P/H

Number of parameters (bytes) = 13

0x1F41

8002

INT16U

4609

A/E/P/H

Destination = 4609 (0x1201)

0x1F42

8003

INT16U

1

A/E/P/H

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

A/E/P/H

Password of the command: Administrator or Operator user profile password

0x1F45

8006

INT16U

1

A/E/P/H

  • 0 = Enable close order

  • 1 = Inhibit close order

0x1F46

8007

INT16U

A/E/P/H

Origin of the command:

256 = command sent via communication interface (IFM or IFE interface)