0613IB1313-10

Time-Stamped Information

General Description

The time-stamped information enables the user to know all the dates related to important information.

The time-stamped information table describes:

  • the current date

  • the last current demand and corresponding dates

  • the last power demand and corresponding dates

  • the last reset and corresponding dates

  • the last k-factor demand peak and corresponding dates

  • the last current demand peak and corresponding dates

Current Date

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x0BB7– 0x0BBA

3000– 3003

R

XDATE

P/H

Current date of the metering manager

0x2327– 0x232A

9000– 9003

R

XDATE

E/P/H

Current date of the protection manager

Last Current Demand

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x0BBC– 0x0BBE

3005–3007

R

DATE

E/P/H

Date of last current demand maximum IA (register 2204)

0x0BBF– 0x0BC1

3008–3010

R

DATE

E/P/H

Date of last current demand maximum IB (register 2205)

0x0BC2– 0x0BC4

3011–3013

R

DATE

E/P/H

Date of last current demand maximum IC (register 2206)

0x0BC5– 0x0BC7

3014–3016

R

DATE

E/P/H

Date of last current demand maximum on the neutral (register 2207) (1)

(1) Value is not available when the system type in register 3314 is 31 or 40. Refer to System Type.

Last Power Demand

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x0BC8– 0x0BCA

3017– 3019

R

DATE

E/P/H

Date of last active power demand maximum (register 2224)

0x0BCB– 0x0BCD

3020– 3022

R

DATE

P/H

Date of last reactive power demand maximum (register 2230)

0x0BCE– 0x0BD0

3023– 3025

R

DATE

E/P/H

Date of last apparent power demand maximum (register 2236)

Last Reset

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x0BD1– 0x0BD3

3026– 3028

R

DATE

P/H

Date of last reset of current demand maximum values

0x0BD4– 0x0BD6

3029– 3031

R

DATE

P/H

Date of last reset of power demand maximum values

0x0BD7– 0x0BD9

3032– 3034

R

DATE

P/H

Date-Time of last min. registers reset (1300–1599) (1)

0x0BDA– 0x0BDC

3035– 3037

R

DATE

P/H

Date-Time of last max. registers reset (1600–1899) (1)

0x0BDD– 0x0BDF

3038– 3040

R

DATE

P/H

Date of last reset of energy meters

0x2331– 0x2333

9010– 9012

R

DATE

P/H

Date of last reset of the maximum phase, ground-fault, and earth-leakage currents

0x236D– 0x236F

9070– 9072

R

DATE

P/H

Date of last reset of the trip history (last 10 faults)

0x2370– 0x2372

9073– 9075

R

DATE

P/H

Date of last reset of the alarm history (last 10 alarms)

(1) This register is updated whenever any of the min. registers are reset. Command interface authorizes user to clear min. of current rms and unbalance values, voltage rms and unbal values, frequency, P/Q/S/PF, fundamental quantities and THD, voltage crest and current crest independently. However, since only one date/time of last reset is maintained, it is recommended to always set all bits in the command that resets min. values.

Last K-Factor Demand Peak

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x0BE0– 0x0BE2

3041–3043

R

DATE

P/H

Date of appearance of last K-factor demand peak (phase A)

0x0BE3– 0x0BE5

3044–3046

R

DATE

P/H

Date of appearance of last K-factor demand peak (phase B)

0x0BE6– 0x0BE8

3047–3049

R

DATE

P/H

Date of appearance of last K-factor demand peak (phase C)

0x0BE9– 0x0BEB

3050–3052

R

DATE

P/H

Date of appearance of last K-factor demand peak (Neutral) (1)

(1) Value is not available when the system type in register 3314 is 31 or 40. Refer to System Type.

Last Current Demand Peak

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x0BEC– 0x0BEE

3053– 3055

R

DATE

P/H

Date of appearance of last I2 demand peak (phase A)

0x0BEF– 0x0BF1

3056– 3058

R

DATE

P/H

Date of appearance of last I2 demand peak (phase B)

0x0BF2– 0x0BF4

3059– 3061

R

DATE

P/H

Date of appearance of last I2 demand peak (phase C)

0x0BF5– 0x0BF7

3062– 3064

R

DATE

P/H

Date of appearance of last I2 demand peak (Neutral) (1)

(1) Value is not available when the system type in register 3314 is 31 or 40. Refer to System Type.