0613IB1313-10

Fault Waveform Capture

General Description

The system stores the variables VAN, VBN, VCN, IA, IB, IC, IN during 12 cycles (16 points per cycles) in the file number 22.

This file consists of a fixed number of records (22). All records are of similar size that is 64 registers wide.

The capture is triggered automatically attached to alarms (1000–1030) by setting the log action to 1.

File Header

The following table describes the file header content:

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x26EB

9964

RW

INT16U

H

File status:

0x0000 = file disabled

0xFFFF = file enabled (factory setting)

0x26EC

9965

R

INT16U

H

Type of file:

22 = fault waveform capture

0x26ED

9966

R

1

INT16U

H

Size of a file = 22 records

0x26EE

9967

R

1

INT16U

H

Size of a record = 64 registers

0x26EF

9968

R

INT16U

1

H

File filling mode:

0 = circular

1 = disabled if log is full

0x26F0

9969

R

1

INT16U

H

Number of cycle segments:

1 = 12 cycles for fault waveform capture

0x26F1

9970

R

1

INT16U

H

Number of cycles before capture:

2 = waveform capture and fault waveform capture

0x26F2

9971

R

1

INT16U

H

Number of points per cycle:

16 = fault waveform capture

File Status

The following table describes the file status content:

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x26FB

9980

R

1

INT16U

H

Size of a file = 22 records

0x26FC

9981

R

1

INT16U

H

Size of a record = 64 registers

0x26FD

9982

R

1

INT16U

H

0x0000 = file OK

0x000A = record size smaller than expected

0x0014 = record size larger than expected

0x001E = insufficient memory

0x00FA = internal error

0x00FD = corrupted allocation table

0x00FE = configuration zero

0x00FF = invalid configuration

0xFC00 = invalid file number

0xFD00 = invalid record number

0xFE00 = file not supported

0xFF00 = cannot allocate file

0x26FE

9983

R

1

INT16U

H

Number of records in the file = 22

0x26FF

9984

R

1

INT16U

P/H

Sequence number of first record in the file (the oldest) = 1

0x2700

9985

R

1

INT16U

P/H

Sequence number of last record in the file (the most recent) = 22

0x2701– 0x2703

9986– 9988

R

DATE

H

Date the last file was reset.

Factory setting = 0x8000 0x8000 0x8000

Fault Waveform Record

The fault waveform capture has a fixed number of records and all record has a fixed number of registers:

Record Number

Registers

Type

Description

1

1–4

XDATE

Extended date/time

5–11

Reserved

12

INT16U

ID of fault WFC trigger: Alarm number 1000 to 1031

13

System type: 31, 40 or 41

14

A

Circuit breaker nominal current

15

SFIXPT

Voltage multiplier for phase A

16

INT16

Voltage offset for phase A

17

SFIXPT

Voltage multiplier for phase B

18

INT16

Voltage offset for phase B

19

SFIXPT

Voltage multiplier for phase C

20

INT16

Voltage offset for phase C

21

SFIXPT

Current multiplier for phase A

22

INT16

Current offset for phase A

23

SFIXPT

Current multiplier for phase B

24

INT16

Current offset for phase B

25

SFIXPT

Current multiplier for phase C

26

INT16

Current offset for phase C

27

SFIXPT

Current multiplier for neutral

28

INT16

Current offset for neutral

29

INT16U

Scaling factor used for SFIXPT math on voltage samples

30

INT16U

Scaling factor used for SFIXPT math on phase current samples

31

INT16U

Scaling factor used for SFIXPT math on neutral current samples

32–64

Not used

2–4

1–64

INT16U

Voltage VAN sample points (16 points - 12 cycles)

5–7

1–64

INT16U

Voltage VBN sample points (16 points - 12 cycles)

8–10

1–64

INT16U

Voltage VCN sample points (16 points - 12 cycles)

11–13

1–64

INT16U

Current IA sample points (16 points - 12 cycles)

14–16

1–64

INT16U

Current IB sample points (16 points - 12 cycles)

17–19

1–64

INT16U

Current IC sample points (16 points - 12 cycles)

20–22

1–64

INT16U

Current IN sample points (16 points - 12 cycles)

Valid only with system type 41

Voltage Calculation

Apply the following rules to derive the voltages:

  • on phase A:

    Sample (Volt) = [(sample – register number 16 of first record) x register number 15 of first record.]/register number 29 of first record.

  • on phase B:

    Sample (Volt) = [(sample – register number 18 of first record) x register number 17 of first record.]/register number 29 of first record.

  • on phase C:

    Sample (Volt) = [(sample – register number 20 of first record) x register number 19 of first record.]/register number 29 of first record.

Current Calculation

Apply the following rules to derive the currents:

  • on phase A:

    Sample (Ampere) = [(sample – register number 22 of first record) x register number 21 of first record.]/register number 30 of first record.

  • on phase B:

    Sample (Ampere) = [(sample – register number 24 of first record) x register number 23 of first record.]/register number 30 of first record.

  • on phase C:

    Sample (Ampere) = [(sample – register number 26 of first record) x register number 25 of first record.]/register number 30 of first record.

  • on neutral:

    Sample (Ampere) = [(sample – register numbr 27 of first record) x register number 28 of first record.]/register number 31 of first record.