0613IB1313-10

IP Network Parameters

Network Parameters

Address

Register

RW

Unit

Type

Range

Description

0x27FF–0x2800

10240–10241

R

INT32

0–1

Network configuration mode:

  • 0 = IPv4 only

  • 1 = IPv4 and IPv6

IPv4 Parameters

Address

Register

RW

Unit

Type

Range

Description

0x2823–0x2824

10276–10277

R-WC

INT32U

0–2

IPv4 address acquisition mode, set by using the EcoStruxure Power Commission software:

  • 0 = Static

  • 1 = BootP

  • 2 = DHCP

0x2825–0x2826

10278–10279

R

INT32U

IPv4 address acquisition status:

  • 0 = IP acquisition successful

  • 1 = IP acquisition in progress

  • 2 = Acquired IP address is duplicated

  • 3 = Error in IP acquisition

0x2827–0x2828

10280–10281

R-WC

INT32U

IPv4 address of IFE interface

Example: 169.254.1.1

Register 10280 = 0xA9FE

Register 10281 = 0x0101

0x2829–0x282A

10282–10283

R-WC

INT32U

IPv4 subnet mask

Example: 255.255.0.0

Register 10282 = 0xFFFF

Register 10283 = 0x0000

0x282B–0x282C

10284–10285

R-WC

INT32U

IPv4 default gateway address

Example: 169.154.1.1

Register 10284 = 0xA9FE

Register 10285 = 0x0101

0x282D–0x2846

10286–10311

Reserved