0613IB1313-10

Protection Event Log

General Description

The system stores the events that concern the protection manager (trips, alarms) in the file number 20.

This file is made up of 100 records and each record is made up of nine registers.

File Header

The following table describes the file header content:

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x26AB

9900

RW

INT16U

P/H

File status:

0x0000 = file disabled

0xFFFF = file enabled (factory setting)

0x26AC

9901

R

INT16U

P/H

Type of file:

20 = protection event log

0x26AD

9902

R

1

INT16U

P/H

Size of a file = 100 records

0x26AE

9903

R

1

INT16U

P/H

Size of a record = 9 registers

0x26AF

9904

R

INT16U

1

P/H

File filling mode:

0 = circular

File Status

The following table describes the file status content:

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x26BB

9916

R

1

INT16U

P/H

Size of a file = 100 records

0x26BC

9917

R

1

INT16U

P/H

Size of a record = 9 registers

0x26BD

9918

R

1

INT16U

P/H

0x0000 = file OK

0x000A = record size smaller than expected

0x0014 = record size larger than expected

0x001E = insufficient memory

0x00FA = internal error

0x00FD = corrupted allocation table

0x00FE = configuration zero

0x00FF = invalid configuration

0xFC00 = invalid file number

0xFD00 = invalid record number

0xFE00 = file not supported

0xFF00 = cannot allocate file

0x26BE

9919

R

1

INT16U

0–100

P/H

Number of records in the file

0x26BF

9920

R

1

INT16U

0–8000

P/H

Sequence number of first record in the file (the oldest)

0x26C0

9921

R

1

INT16U

0–8000

P/H

Sequence number of last record in the file (the most recent)

0x26C1– 0x26C3

9922– 9924

R

DATE

P/H

Date the last file was reset.

Factory setting = 0x8000 0x8000 0x8000

Protection Event Record

The following table shows the format of 1 record in the protection event log.

Registers

Type

Bits

Description

1–4

XDATE

Event date

5

INT16U

Event number: alarm code or trip code

6

INT16U

Event characteristics for protection event log (1)

7

INT16U

0–7

1 = event of the over type

2 = alarm of the under type

3 = alarm of the minimum type

4 = alarm of the maximum type

5 = alarm of the assorted type

8–11

1 = start of an event

2 = end of an alarm

12–15

Alarms 1100–1106 have a priority 3. For other alarms, the value contained in these 4 bits represents the priority linked to the event (if applicable and depending on the alarm configuration).

8

INT16U

Logging register associated to the alarm (2)

9

INT16U

Action register associated to the alarm (2)

(1) For event numbers 1000–1004, the data is the value of the fault current interrupted by the circuit breaker.

For all other protection events, this value is forced to 32768.

(2) Registers 8 and 9 are a copy of the alarm configuration registers at the moment the event occurred. These registers depend entirely on the user configurations. For the events 1100–1106, these registers are forced to 32768.