Schematics with MasterPact NT/NW and PowerPact P- and R-Frame Circuit Breakers
General Description
Depending on the type of circuit breaker used, the IFM interface must be connected to the circuit breaker by using one of the following configurations:
-
Connect the IFM interface to a fixed manually-operated PowerPact P- or R-frame circuit breaker with a BCM ULP module.
-
Connect the IFM interface to a fixed electrically-operated MasterPact NT/NW or PowerPact P- or R-frame circuit breaker with a BCM ULP module.
-
Connect the IFM interface to a drawout MasterPact NT/NW or PowerPact P- or R-frame circuit breaker with a BCM ULP module and their respective IO module.
For more information, refer to the ULP System User Guide.
ULP Connection
| NOTICE |
|---|
|
HAZARD OF EQUIPMENT DAMAGE
Failure to follow these instructions can result in equipment damage.
|
All the connection configurations require the circuit breaker BCM ULP cord. The insulated NSX cord is mandatory for system voltages greater than 480 Vac.
Connection of the IFM Interface to a Fixed Manually-Operated PowerPact P- or R-Frame Circuit Breaker
Connection of the IFM Interface to a Fixed Electrically-Operated MasterPact NT/NW or PowerPact P- or R-Frame Circuit Breaker
Connection of the IFM Interface to a Drawout MasterPact NT/NW or PowerPact P- or R-Frame Circuit Breaker

A IFM Modbus-SL interface for one circuit breaker
B RJ45 ULP cord ULP cord
C Circuit breaker BCM ULP cord
D Circuit breaker disconnected position contact (CD)
E Circuit breaker cradle
F BCM ULP circuit breaker communication module
G Drawout circuit breaker
H Drawout terminal block
I Circuit breaker connected position contact (CE)
J Circuit breaker test position contact (CT)
K IO input/output application module for one circuit breakers (IO module)