Basic Protection Parameters
Neutral Protection Parameters
The neutral protection is only available when system type in register 3314 is 30 or 41.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x2230 |
8753 |
RW |
1 |
– |
INT16U |
0–3 |
A/E/P/H |
Type of neutral protection: (1) 0 = OFF 1 = N/2 (Ir/2) 2 = N (Ir) 3 = Nx1.6 (1.6 Ir) (2) |
|
(1) Write Access only with MicroLogic P and H trip unit. (2) Value accessible only for MicroLogic P and H trip unit. |
||||||||
Long-Time Protection Parameters
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x2231 |
8754 |
R |
– |
– |
INT16U |
0–1 |
A/E/P/H |
– |
Status: 0x0001 = On |
|
0x2232 |
8755 |
RW |
– |
– |
INT16U |
– |
– |
– |
Type of IDMTL curve (1) |
|
A/E/P/H |
0 |
Standard long-time curve I2t (factory setting) |
|||||||
|
P/H |
1 |
SIT curve |
|||||||
|
P/H |
2 |
VIT curve |
|||||||
|
P/H |
3 |
EIT (I2t on) curve |
|||||||
|
P/H |
4 |
HVF curve |
|||||||
|
P/H |
5 |
Constant time (I2t off) |
|||||||
|
– |
6–15 |
Reserved |
|||||||
|
0x2233– 0x2234 |
8756– 8757 |
RW |
1 |
A |
MOD 10000 |
40– 8000 |
A/E/P/H |
– |
Ir pick-up value (1) |
|
0x2235 |
8758 |
RW |
1 |
ms |
INT16U |
500– 24000 |
A/E/P/H |
– |
tr time delay (1) |
|
0x2236– 0x2238 |
8759– 8761 |
– |
– |
– |
– |
– |
– |
– |
Reserved |
|
0x2239 |
8762 |
RW |
– |
– |
INT16U |
– |
H |
– |
Waveform capture setting: 0 = no waveform capture 0x0100 = waveform capture into the Fault Waveform Capture file no. 22 at the end of the time delay tr. |
|
0x223A |
8763 |
RW |
– |
– |
INT16U |
– |
– |
– |
M2C/M6C programmable contact setting: Bit set to 1 = contact closed at the end of the time delay tr (factory setting) Bit set to 0 = contact open at the end of the time delay tr |
|
– |
0 |
Always set to 1 |
|||||||
|
– |
1–7 |
Reserved |
|||||||
|
E/P/H |
8 |
Contact 1 |
|||||||
|
E/P/H |
9 |
Contact 2 |
|||||||
|
P/H |
10 |
Contact 3 |
|||||||
|
P/H |
11 |
Contact 4 |
|||||||
|
P/H |
12 |
Contact 5 |
|||||||
|
P/H |
13 |
Contact 6 |
|||||||
|
– |
14–15 |
Reserved |
|||||||
|
(1) Write Access only with MicroLogic P and H trip unit. |
|||||||||
Short-Time Protection Parameters
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x223B |
8764 |
R |
– |
– |
INT16U |
0–1 |
A/E/P/H |
– |
Status: 0x0001 = On |
|
0x223C |
8765 |
RW |
– |
– |
INT16U |
0–1 |
A/E/P/H |
– |
Type of protection: (1) 0 = I2t On 1 = I2t Off |
|
0x223D– 0x223E |
8766– 8767 |
RW |
1 |
A |
MOD 10000 |
60– 80 000 |
A/E/P/H |
– |
Isd pick-up value (1) |
|
0x223F |
8768 |
RW |
1 |
ms |
INT16U |
0–400 |
A/E/P/H |
– |
tsd time delay (1) 0 s: valid only for the I²t off position 100–400 ms: valid for the I²t on and I²t off positions |
|
0x2243 |
8772 |
RW |
– |
– |
INT16U |
– |
H |
– |
Waveform capture setting: 0 = no waveform capture 0x0100 = waveform capture into the Fault Waveform Capture file at the end of the time delay tsd. |
|
0x2244 |
8773 |
RW |
– |
– |
INT16U |
– |
– |
– |
M2C/M6C programmable contact setting: Bit set to 1 = contact closed at the end of the time delay tsd (factory setting) Bit set to 0 = contact open at the end of the time delay tsd |
|
– |
0 |
Always set to 1 |
|||||||
|
– |
1–7 |
Reserved |
|||||||
|
E/P/H |
8 |
Contact 1 |
|||||||
|
E/P/H |
9 |
Contact 2 |
|||||||
|
P/H |
10 |
Contact 3 |
|||||||
|
P/H |
11 |
Contact 4 |
|||||||
|
P/H |
12 |
Contact 5 |
|||||||
|
P/H |
13 |
Contact 6 |
|||||||
|
– |
14–15 |
Reserved |
|||||||
|
(1) Write Access only with MicroLogic P and H trip unit. |
|||||||||
Instantaneous Protection Parameters
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x2245 |
8774 |
R |
– |
– |
INT16U |
0x0001–0x0101 |
A/E/P/H |
– |
0x0001 = protection active (factory setting) 0x0101 = protection OFF |
|
0x2246 |
8775 |
– |
– |
– |
– |
– |
– |
– |
Reserved |
|
0x2247– 0x2248 |
8776– 8777 |
RW |
1 |
A |
MOD 10000 |
200– 120000 |
A/E/P/H |
– |
I pick-up value for the instantaneous protection (1) |
|
0x2249 |
8778 |
– |
– |
– |
– |
– |
– |
– |
Reserved |
|
0x224D |
8782 |
RW |
– |
– |
INT16U |
– |
H |
– |
Waveform capture setting: 0 = no waveform capture 0x0100 = waveform capture into the Fault Waveform Capture file at the end of the time delay. |
|
0x224E |
8783 |
RW |
– |
– |
INT16U |
– |
– |
– |
M2C/M6C programmable contact setting: Bit set to 1 = contact closed at the end of the time delay (factory setting) Bit set to 0 = contact open at the end of the time delay |
|
– |
0 |
Always set to 1 |
|||||||
|
– |
1–7 |
Reserved |
|||||||
|
E/P/H |
8 |
Contact 1 |
|||||||
|
E/P/H |
9 |
Contact 2 |
|||||||
|
P/H |
10 |
Contact 3 |
|||||||
|
P/H |
11 |
Contact 4 |
|||||||
|
P/H |
12 |
Contact 5 |
|||||||
|
P/H |
13 |
Contact 6 |
|||||||
|
– |
14–15 |
Reserved |
|||||||
|
(1) Write Access only with MicroLogic P and H trip unit. |
|||||||||
Ground-Fault Protection Parameters
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x224F |
8784 |
RW |
– |
– |
INT16U |
0x0001–0x0101 |
A/E/P/H |
– |
Protection status: (1) (2) 0x0001 = protection active (factory setting) 0x0101 = protection OFF |
|
0x2250 |
8785 |
RW |
– |
– |
INT16U |
0–1 |
A/E/P/H |
– |
Type of protection: (1) 0 = I2t On 1 = I2t Off |
|
0x2251– 0x2252 |
8786– 8787 |
RW |
1 |
A |
MOD 10000 |
30– 1200 |
A/E/P/H |
– |
Ig pickup for the ground-fault protection (1) |
|
0x2253 |
8788 |
RW |
1 |
ms |
INT16U |
0–400 |
A/E/P/H |
– |
tg tripping time delay for the ground-fault protection: (1) 0 s = valid only for the I2t off position 100–400 ms = valid for the I2t on and I2t off positions |
|
0x2257 |
8792 |
RW |
– |
– |
INT16U |
– |
H |
– |
Waveform capture setting: 0 = no waveform capture 0x0100 = waveform capture into the Fault Waveform Capture file at the end of the time delay tg. |
|
0x2258 |
8793 |
RW |
– |
– |
INT16U |
– |
– |
– |
M2C/M6C programmable contact setting: Bit set to 1 = contact closed at the end of the time delay tg (factory setting) Bit set to 0 = contact open at the end of the time delay tg |
|
– |
0 |
Always set to 1 |
|||||||
|
– |
1–7 |
Reserved |
|||||||
|
E/P/H |
8 |
Contact 1 |
|||||||
|
E/P/H |
9 |
Contact 2 |
|||||||
|
P/H |
10 |
Contact 3 |
|||||||
|
P/H |
11 |
Contact 4 |
|||||||
|
P/H |
12 |
Contact 5 |
|||||||
|
P/H |
13 |
Contact 6 |
|||||||
|
– |
14–15 |
Reserved |
|||||||
|
(1) Write Access only with MicroLogic P and H trip unit. (2) In order to be able to write this register, the following conditions must be met:
|
|||||||||
Earth-Leakage (Vigi) Protection Parameters
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x2259 |
8794 |
R |
– |
– |
INT16U |
0x0001 |
A/P/H |
– |
0x0001 = protection active |
|
0x225A |
8795 |
– |
– |
– |
– |
– |
– |
– |
Reserved |
|
0x225B– 0x225C |
8796– 8797 |
RW |
1 |
mA |
MOD 10000 |
5–300 |
A/P/H |
– |
IΔn pickup for the earth-leakage protection (1) |
|
0x225D |
8798 |
RW |
1 |
ms |
INT16U |
0–1000 |
A/P/H |
– |
Δt tripping time delay for the earth-leakage protection (1) |
|
0x2261 |
8802 |
RW |
– |
– |
INT16U |
– |
H |
– |
Waveform capture setting: 0 = no waveform capture 0x0100 = waveform capture into the Fault Waveform Capture file at the end of the time delay Δt. |
|
0x2262 |
8803 |
RW |
– |
– |
INT16U |
– |
P/H |
– |
M2C/M6C programmable contact setting: Bit set to 1 = contact closed at the end of the time delay Δt (factory setting) Bit set to 0 = contact open at the end of the time delay Δt |
|
– |
0 |
Always set to 1 |
|||||||
|
– |
1–7 |
Reserved |
|||||||
|
P/H |
8 |
Contact 1 |
|||||||
|
P/H |
9 |
Contact 2 |
|||||||
|
P/H |
10 |
Contact 3 |
|||||||
|
P/H |
11 |
Contact 4 |
|||||||
|
P/H |
12 |
Contact 5 |
|||||||
|
P/H |
13 |
Contact 6 |
|||||||
|
– |
14–15 |
Reserved |
|||||||
|
(1) Write Access only with MicroLogic P and H trip unit. |
|||||||||