DOCA0285EN-04

Locking the MasterPacT MTZ2 Safety Shutters

Using Shutter Position Indication and Locking Accessory

Step

Action

1

The shutter indicator arms can be locked individually or together:

  • To lock the top safety shutter, pull the left shutter indicator arm tab out of the slot.

  • To lock the bottom safety shutter, pull the right shutter indicator arm tab out of the slot.

2

Insert the padlock in the padlock tab and close the padlock.

3

Check that the bottom safety shutters do not open when the actuator on the right is pressed.

Using Shutter Locking Blocks

Step

Action

1

Remove the shutter locking blocks stored in the chassis.

2

Place the shutter locking blocks in the appropriate guides:

  • To lock the top safety shutter, install a shutter locking block on the shutter mechanism on the left.

  • To lock the bottom safety shutter, install a shutter locking block on the shutter mechanism on the right.

3

Insert a padlock in each shutter locking block tab and close the padlock.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?