DOCA0285EN-04

Operating Conditions

@experts: Topic shared between DOCA0284 and DOCA0285, with profiling; indicate if comments do not apply to both guides

Introduction

MasterPacT MTZ circuit breakers are designed and tested for operation in industrial atmospheres. It is recommended that equipment is cooled or heated to the proper operating temperature and kept free of excessive vibration and dust.

Ambient Temperature

MasterPacT MTZ circuit breakers can operate under the following temperature conditions:

  • Electrical and mechanical characteristics specified for an ambient temperature of -25 °C to +70 °C.

  • Circuit-breaker closing specified down to -35 °C by manual operation with closing pushbutton.

Storage conditions are as follows:

  • -40 °C to +85 °C for the circuit breaker without the control unit.

  • -25 °C to +85 °C for the control unit.

Extreme Atmospheric Conditions

MasterPacT MTZ circuit breakers have successfully passed tests for extreme atmospheric conditions, defined by the following standards:

Standard

Title

IEC 60068-2-1

Dry cold, at -40 °C

IEC 60068-2-2

Dry heat, at +85 °C

IEC 60068-2-30

Damp heat (temperature +55 °C, relative humidity 95%)

IEC 60068-2-52 level 2

Salt mist

Industrial Environments

MasterPacT MTZ circuit breakers can operate in the industrial environments defined by IEC 60947 (pollution degree up to 3).

It is advisable to check that circuit breakers are installed in suitably cooled switchboards without excessive dust.

Conditions

Standard

Corrosive industrial atmospheres

Category 3C3 compliant with IEC 60721-3-3

Sea salts 0.8 to 8 mg/m² day average over the year

Compliant with IEC 60721-2-5

Mechanically active substances

Category 3S3 compliant with IEC 60721-3-3

Beyond these conditions, MasterPacT MTZ circuit breakers must be installed inside switchboards with an IP rating equal to or greater than IP54.

Vibration

MasterPacT MTZ circuit breakers have successfully passed tests for the following vibration levels, in compliance with IEC 60068-2-6 and IEC 60068-2-27:

  • 2 Hz to 13.2 Hz: amplitude +/- 1 mm.

  • 13.2 Hz to 100 Hz: constant acceleration of 0.7 g.

Vibration testing to these levels is required by merchant marine inspection organizations (for example, Veritas, Lloyd’s).

MasterPacT MTZ circuit breakers have also been successfully tested according to:

  • Annex Q - IEC 60947-1: Special tests – damp heat, salt mist, vibration and shock

  • IEC 60947-1 - Category D: Environment subject to temperature, humidity and vibration

Altitude

MasterPacT MTZ circuit breakers are designed and tested to operate at altitudes below 2,000 m.

At altitudes above 2,000 m, the characteristics of the ambient air (electrical resistance, cooling capacity) lower product characteristics as follows:

Characteristics

Altitude

2,000 m

3,000 m

4,000 m

5,000 m

Impulse withstand voltage Uimp (kV)

12

11

10

8

Rated insulation voltage (Ui) (V)

1,000

900

780

700

Maximum rated operational voltage 50/60 Hz Ue (V)

690

690

630

560

Rated current (A) at 40 °C

1 x In

0.99 x In

0.96 x In

0.94 x In

NOTE: Intermediate values can be obtained by interpolation.

Electromagnetic Disturbances

MasterPacT MTZ circuit breakers have protection against:

  • Overvoltages caused by circuit breakers that generate electromagnetic disturbance.

  • Overvoltages caused by atmospheric disturbance or by a distribution-system outage (for example, a lighting system failure).

  • Circuit breakers emitting radio waves (for example, radio transmitters, walkie-talkies, or radar).

  • Electrostatic discharge produced by users.

MasterPacT MTZ circuit breakers have successfully passed the electromagnetic-compatibility tests (EMC) defined by the following international standards:

  • IEC 60947-2, appendix F.

  • IEC 60947-2, appendix B (control units with earth-leakage function).

The circuit breakers have passed the above tests and therefore:

  • No nuisance tripping occurs.

  • Tripping times are respected.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?