DOCA0285EN-04

Chassis Locking in Any Position

@experts: Topic shared between DOCA0284 and DOCA0285, with profiling; indicate if comments do not apply to both guides

Description

The chassis can be locked in any position (connected, test, or disconnected position).

This locking function requires a mechanical adaptation of the chassis, explained in the following procedure.

When the chassis is locked, the racking handle cannot be inserted in the racking handle socket.

The chassis can be locked in any position:

  • By up to three padlocks with shackle diameter 5-8 mm as standard.

  • By one or two optional keylocks.

Keylocks can be used in addition to padlocks.

VSPD Chassis Locking by Keylock Accessory

The chassis locking by keylock accessory and the locking and unlocking procedures are the same as for the chassis locking in disconnected position.

Adapting the Chassis

DANGER
HAZARD OF DEVICE FALLING
  • Be sure that lifting equipment has lifting capacity for the device being lifted.
  • Follow manufacturer’s instructions for use of lifting equipment.
  • Wear hard hat, safety shoes, and heavy gloves.
Failure to follow these instructions will result in death or serious injury.
NOTICE
HAZARD OF EQUIPMENT DAMAGE
The chassis must be securely fastened when installing or removing the device.
Failure to follow these instructions can result in equipment damage.

Follow this procedure to adapt the chassis locking mechanism so that the chassis can be locked in any position.

Step

Action

1

Make sure that chassis indicator is in the disconnected position.

2

Remove the circuit breaker from the chassis.

3

Insert the racking handle into the racking handle socket.

4

Rotate the latch to the front.

The chassis can now be locked in any position.

NOTE: To return the chassis to locking only in the disconnected position, rotate the latch to its original position at the rear.

Latch position for locking in disconnected position

Latch position for locking in any position

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?