Opening the Circuit Breaker
Opening Conditions
To open the circuit breaker, the circuit breaker must be closed ().
Opening the Circuit Breaker
The following tables present the different ways to open the circuit breaker in the different control modes available.
The circuit breaker can be opened in the following ways in all control modes:
Additionally, the circuit breaker can be opened in the following ways when Auto Local or Auto Remote control mode is configured:
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
|
Opening type |
Control mode |
Accessories |
Opening action |
|---|---|---|---|
|
Through BCIM module |
Auto Local |
|
Press the external pushbutton which is connected to the MX communicating opening voltage release via a BCIM IO channel. This opening action is only allowed when:
|
|
Through FDM121 display |
Auto Local |
|
Send a command to open the circuit breaker from FDM121 display connected locally to the circuit breaker through the ULP system. This opening action is only allowed when Auto Local control mode is configured. |
|
Through Modbus communication |
Auto Remote |
|
Send a command to open the circuit breaker through the Modbus communication network. This opening action is only allowed when Auto Remote control mode is configured. Refer to DOCA0384•• MasterPacT, ComPacT, PowerPacT Circuit Breakers - Modbus Communication - User Guide in Related Documents at the beginning of this guide. |
|
Through IFE/EIFE webpages |
Auto Remote |
|
Send a command to open the circuit breaker from the IFE/EIFE control webpage. This opening action is only allowed when Auto Remote control mode is configured. Refer to the relevant document in Related Documents at the beginning of this guide:
|
If the circuit breaker does not open, refer to MasterPacT MTZ Troubleshooting.
DANGER