DOCA0285EN-04

Removing the Drawout Circuit Breaker

@experts: Topic shared between DOCA0284 and DOCA0285, with profiling; indicate if comments do not apply to both guides

Circuit Breaker Removal

NOTICE
HAZARD OF EQUIPMENT DAMAGE
The chassis must be securely fastened when installing or removing the device.
Failure to follow these instructions can result in equipment damage.

Step

Action

1

With the circuit breaker in the disconnected position, discharge the closing spring by pressing the closing pushbutton.

If the closing spring is charged, the circuit breaker closes.

NOTE: For drawout circuit breakers fitted with the optional DAE automatic spring-discharge interlock, the closing spring is discharged when the circuit breaker is moved from disconnected to withdrawn position.

2

Press the opening pushbutton to open the circuit breaker.

3

Press and hold the rail release tabs towards the back.

4

Pull out the rails to the maximum by pulling on the drawout grips.

Result: The circuit breaker is supported on the rails, clear of the chassis and ready to be lifted.

Lifting the Circuit Breaker

Both the circuit breaker and chassis have a carrying grip for lifting. To lift the circuit breaker, use an overhead lifting device attached to the carrying grip, following the directions given in this section.

DANGER
HAZARD OF DEVICE FALLING
  • Be sure that lifting equipment has lifting capacity for the device being lifted.
  • Follow manufacturer’s instructions for use of lifting equipment.
  • Wear hard hat, safety shoes, and heavy gloves.
Failure to follow these instructions will result in death or serious injury.

Lift the circuit breaker from the chassis rails by using the carrying grip located on the sides of the circuit breaker.

Circuit Breaker Weights

The following table shows the weights of the different circuit breakers available.

Number of poles

Circuit breaker

MTZ2

MTZ3

3P

Moving part (Drawout)

50 kg

120 kg

Chassis

40 kg

105 kg

Fixed circuit breaker

50 kg

120 kg

4P

Moving part (Drawout)

65 kg

160 kg

Chassis

55 kg

140 kg

Fixed circuit breaker

65 kg

160 kg

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?