Engaging/Disengaging the ERMS Function
Presentation
The ERMS function is used to reduce protection settings so that the circuit breaker trips as soon as possible when an electrical fault occurs. Minimizing the time between the electrical fault and circuit breaker trip helps to reduce the risk of injury when qualified electrical personnel are near energized equipment.
When the ERMS function is engaged, the ERMS protection settings replace the standard protection settings.
Availability
The ERMS function is available on MicroLogic Active 2.0, 5.0 and 6.0 control units for IEC standard.
Operating Principle
The ERMS function can be engaged or disengaged by using the ERMS button, or by using an external selector switch connected to the BCIM module.
|
While the ERMS function is engaged:
|
For more information about the ERMS function, and how to engage and disengage the ERMS function, refer to DOCA0265•• MasterPacT MTZ - MicroLogic Active Control Unit - User Guide in Related Documents at the beginning of this guide.
Engaging the ERMS Function
DANGER |
|---|
|
hazard of incorrect ERMS status
Failure to follow these instructions will result in death or serious injury.
|
The ERMS can be engaged in different ways, according to the circuit breaker configuration and its accessories:
|
Type |
Accessories |
Action |
|---|---|---|
|
Through the ERMS button on MicroLogic Active control unit |
– |
Press the ERMS button to engage the ERMS function. |
|
Through an external selector switch connected to the BCIM module |
|
Turn the external selector switch to the Engaged position. The BCIM module must be configured in ERMS mode. |
Disengaging the ERMS Function
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Prior to disengaging ERMS:
Failure to follow these instructions will result in death or serious injury.
|
The way to disengage the ERMS function depends on how it was engaged:
|
Type |
Accessories |
Action |
|---|---|---|
|
Through the ERMS button on MicroLogic Active control unit |
– |
Press the ERMS button to disengage the ERMS function. |
|
Through an external selector switch connected to the BCIM module |
|
Turn the external selector switch to the Disengaged position. |
DANGER