DOCA0285EN-04

Mismatch Protection

@experts: Topic shared between DOCA0284 and DOCA0285, with profiling; indicate if comments do not apply to both guides

Description

Mismatch protection allows the installation of a MasterPacT MTZ2/MTZ3 circuit breaker only in a chassis with compatible characteristics.

Mismatch protection offers 35 different combinations that can be selected so that a circuit breaker can only be mounted on a chassis with the matching combination.

Accessory

The use of mismatch protection is optional. One mismatch protection accessory is required for each circuit breaker.

For information on the accessory installation, consult the instruction sheet available at Schneider Electric website: NVE35465.

Pin Location of Mismatch Protection

The following illustration shows the pin location on the chassis and circuit breaker, respectively.

The pin combination selected on the chassis must correspond to the pin combination selected on the circuit breaker (see following table). For example, the combination ABCD on the chassis corresponds to the combination 567 on the circuit breaker.

Pins on the chassis are labeled A, B, C, D, E, F, G.

Pins on the circuit breaker are labeled 1, 2, 3, 4, 5, 6, 7.

Recommended Pin Combinations

The following are the recommended pin combinations:

Pins on chassis

Pins on circuit breaker

Pins on chassis

Pins on circuit breaker

ABCD

567

BCDE

167

ABCE

467

BCDF

157

ABCF

457

BCDG

156

ABCG

456

BCEF

147

ABDE

367

BCEG

146

ABDF

357

BCFG

145

ABDG

356

BDEF

137

ABEF

347

BDEG

136

ABEG

346

BDFG

135

ABFG

345

BEFG

134

ACDE

267

CDEF

127

ACDF

257

CDEG

126

ACDG

256

CDFG

125

ACEF

247

CEFG

124

ACEG

246

DEFG

123

ACFG

245

   

ADEF

237

   

ADEG

236

   

ADFG

235

   

AEFG

234

   
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?