DOCA0285EN-04

Circuit Breaker Interlocking Actions

@experts: Topic shared between DOCA0284 and DOCA0285, with profiling; indicate if comments do not apply to both guides

About Interlocking Actions

An interlocking action is an automatic locking operation provided by interlocking accessories added to the MasterPacT MTZ2/MTZ3 circuit breaker or chassis.

A number of optional interlocking accessories are available for the MasterPacT MTZ2/MTZ3 circuit breaker and chassis. For a complete listing of available interlocks, refer to LVPED225010EN MasterPacT MTZ with MicroLogic Active Control Unit - Catalog in Related Documentsat the beginning of this guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?