DOCA0285EN-04

Mechanical Interlocking for Transfer Switches

@experts: Topic shared between DOCA0284 and DOCA0285, with profiling; indicate if comments do not apply to both guides

Description

The mechanical interlocking for transfer switches between MasterPacT MTZ circuit breakers prevents the interlocked circuit breakers from closing at the same time. The following interlocking functions are available:

  • Interlocking between two circuit breakers

  • Interlocking between three circuit breakers:

    • Three incomers

    • Two incomers and one coupling

    • Two incomers and one replacement

VBP Pushbutton Locking Accessory

The VBP pushbutton locking accessory provides redundancy in addition to the mechanical interlocking system.

The use of the pushbutton locking cover is mandatory on each interlocked MasterPacT MTZ circuit breaker. The closing pushbuttons of the interlocked circuit breakers must be locked by padlocks sharing one key to help avoid simultaneous closing orders of interlocked circuit breakers.

For more information about the pushbutton locking cover, refer to VBP Pushbutton Locking Accessory.

Mechanical Interlocking Between Two Circuit Breakers

Two circuit breakers can be mechanically interlocked by cables or by rods so that both circuit breakers cannot be closed at the same time.

For information on the accessory installation, consult the instruction sheet on the Schneider Electric website:

Mechanical Interlocking Between Three Incomers

Mechanical interlocking is between three main circuit breakers connected to different power sources.

Only one of the three circuit breakers can be in the closed position at a time. The other two circuit breakers are held in the locked open position.

For information on the accessory installation, consult the instruction sheet on the Schneider Electric website: NVE35498

Mechanical Interlocking Between Two Incomers and One Coupling

Mechanical interlocking is between two main circuit breakers connected to different power sources and one tie circuit breaker.

Two of the three circuit breakers can be in the closed position at any time.

(1) Possible by forcing operation

For information on the accessory installation, consult the instruction sheet on the Schneider Electric website: NVE35500

Mechanical Interlocking Between Two Incomers and One Replacement

Mechanical interlocking is between two main circuit breakers connected to the same power source and a third circuit breaker connected to a generator power source.

The generator circuit breaker is locked open when either or both of the main circuit breakers are closed.

For information on the accessory installation, consult the instruction sheet on the Schneider Electric website: NVE35499

IVE Electrical Interlocking Unit

Electrical interlocking between MasterPacT MTZ circuit breakers can be done using the IVE electrical interlocking unit or by using dedicated wiring. The IVE unit is suitable for two circuit breakers only. For three circuit breakers, dedicated wiring is required to perform the electrical interlocking.

For information on the accessory installation, consult the instruction sheet on the Schneider Electric website: 51201201AA

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?