DOCA0285EN-04

VPOC Open-door Racking Interlock

@experts: Topic shared between DOCA0284 and DOCA0285, with profiling; indicate if comments do not apply to both guides

Description

With the racking interlock installed, a drawout MasterPacT MTZ2/MTZ3 circuit breaker cannot be racked in or out when the equipment door is open because the racking handle cannot be inserted.

Accessory

The optional VPOC racking interlock can be installed on the right side of the chassis.

For information on the accessory installation, consult the instruction sheet on the Schneider Electric website: NVE35494.

Activating the Racking Interlock

Step

Action

1

Insert the racking interlock.

2

Check that the racking handle cannot be inserted into the racking handle socket when the equipment door is open.

3

Check that the racking handle can be inserted into the racking handle socket when the equipment door is closed.

Deactivating the Racking Interlock

Step

Action

1

Pull out the racking interlock.

2

Check that the racking handle can be inserted into the racking handle socket when the equipment door is open or closed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?