DOCA0285EN-04

Troubleshooting: Control Operations from Wired Communication Network

Definition

Control operations include commands to open and close the device from the wired communication network.

For information about control operations from the wired communication network, refer to DOCA0384•• MasterPacT, ComPacT, PowerPacT Circuit Breakers - Modbus Communication - User Guide in Related Documents at the beginning of this guide.

Device Cannot be Controlled with a Remote Controller Connected from IFE, EIFE or IFM Interface

Problem description

Symptom

Probable causes

Solutions

Device cannot be opened or closed.

The device control mode is set to Manual or Auto Local.

Change the control mode to Auto Remote.

 

The remote control commands are disabled by the locking pad on the front of the IFE interface.

Move the locking pad on the front of the IFE interface to the Unlocked position.

 
 

Additional Checks

If the troubleshooting actions described above do not work, refer to the troubleshooting information for Mechanical Control Operations and Electrical Control Operations.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?