DOCA0285EN-04

Drawout Circuit Breaker

@experts: Topic shared between DOCA0284 and DOCA0285, with profiling; indicate if comments do not apply to both guides

Definition

A drawout circuit breaker is composed of the moving part (also called the circuit breaker) and the fixed part (or chassis).

Drawout Circuit Breaker Moving Part Description

The following image shows the standard version of the moving part of a drawout circuit breaker (no optional accessories).

A Carrying grip

B Arc chute

C Blue fault-trip reset button

D Product identification label, with manufacturing date

E Opening pushbutton

F Closing pushbutton

G Spring charging handle

H Terminal block connectors

I Front cover

J VBP pushbutton locking cover (optional)

K Rating plate

L Spring charged and ready-to-close indicator

M Main-contact position indicator

N Window to consult the (optional) CDM mechanical operation counter

O Control unit

P Control unit transparent cover

Drawout Circuit Breaker Accessories Description

The following image shows the accessories available for the moving part of a drawout circuit breaker.

A VDC mismatch protection

B Terminal block connectors for optional accessories

C Terminal block connectors for standard accessories

D Optional block of four OF indication contacts or EF combined connected/closed contacts

E Four OF indication contacts (delivered as standard)

F KMT grounding kit

G MCH gear motor

H CDM mechanical operation counter

Z1, Z2 See following images

The following images zoom in on the accessories for the moving part of a drawout circuit breaker.

I Standard SDE1 fault-trip indication contact

J Optional SDE2 fault-trip indication contact or RES electrical remote reset

K Microswitch

L BCIM module

M MN undervoltage release or MX2 opening voltage release

N MX1 opening voltage release

O PF ready-to-close contact

P XF closing voltage release

Q VCPO OFF-position locking by padlocks

R VSPO OFF-position locking by keylocks

Chassis Description

The following image shows the standard version of the chassis (no optional accessories).

A Carrying grip

B Terminal blocks supplied as standard

C Terminal block identification plate

D Top safety shutter

E Bottom safety shutter

F Rail release tab

G Drawout grip

H Extension rail

I Racking handle storage space

J Racking handle

K Moving part position indicator

L Racking handle socket

M Position release button

N Chassis locking by padlocks

O Latch for switching chassis locking from disconnected position to any position (connected, test, disconnected)

P Shutter locking block

Chassis Accessories Description

The following image shows the accessories available for the chassis.

A VDC mismatch protection

B Drawout device position contacts

C ULP port

D Optional terminal block

E Cord between ULP port module and EIFE interface

F EIFE embedded Ethernet interface

G Circuit breaker auxiliary terminal shield

H VPOC open-door racking interlock

I VIVC shutter position indication and locking

J IBPO interlock between racking handle and opening pushbutton

K VSPD chassis locking by keylocks

L VPEC door interlock

Chassis Terminal Block Description

Terminal block supplied as standard on the chassis

Optional terminal block on the chassis

NOTE: Two markings are possible for the COM and UC3 terminal blocks.
 

Old marking

New marking

 

(1) Supplied as standard with chassis for MasterPacT MTZ2/MTZ3 circuit breakers only

(2) Supplied as standard with 3P chassis only

Assignment of Chassis Terminal Blocks

DANGER
HAZARD OF ELECTROCUTION FOR VOLTAGES ABOVE 480 VAC
If a voltage greater than 480 Vac is connected to a terminal, it is forbidden to connect adjacent terminals to a 24 Vdc SELV (Safety Extra Low Voltage) power supply in order to observe the insulation distances. For example, if you connect a 690 Vac supply to the UC4 terminal block, you must not connect a 24 Vdc SELV supply to the SDE2 terminal block.
Failure to follow these instructions will result in death or serious injury.

The following table describes the assignment and the availability of the terminal blocks for drawout circuit breakers:

  • Standard terminal blocks are delivered on the chassis, even if the associated accessories are not installed in the circuit breaker.

  • Optional terminal blocks are delivered on the chassis only if the associated optional accessories are installed in the circuit breaker.

Block

Marking

Description

Availability

A

CD1–CD3

CE4–CE6

3 CD disconnected position contacts

or 3 CE connected position contacts

Optional

B

COM

MicroLogic Active without BCIM module:

  • Terminal block for the external power supply of the MicroLogic Active control unit

Standard

MicroLogic Active with BCIM module:

  • Terminal block for the connection of the BCIM module to ULP modules, by using the circuit breaker ULP cord

  • or ULP port module for the connection of the BCIM module to ULP modules, by using a ULP cord

Optional

UC1

Zone selective interlocking (ZSI)

Standard

UC2

Neutral external sensor

Standard

SDE2/RES

SDE2 additional fault-trip indication contact or RES electrical remote reset

Optional

UC4

MicroLogic Active without BCIM module:

  • External phase voltage

MicroLogic Active with BCIM module:

  • External phase voltage

  • or 2 BCIM IO channels

Optional

UC3

MicroLogic Active without BCIM module:

  • External neutral voltage

MicroLogic Active with BCIM module:

  • External neutral voltage and external power supply of the MicroLogic Active control unit

Standard on 3P circuit breakers

Optional on 4P circuit breakers

M2C/ESM

M2C or ESM: not applicable

Optional

SDE1

SDE1 fault-trip indication contact

Standard

CE1–CE3

CT4–CT6

3 CE connected position contacts

or 3 CT test position contacts

Optional

C

MN/MX2

MN undervoltage release or MX2 opening voltage release

Standard

MX1

MX1 opening voltage release

Standard

XF

XF closing voltage release

Standard

PF

PF ready-to-close contact

Standard

MCH

MCH gear motor

Standard

D (without EIFE interface)

OF11–OF24

EF11–EF24

8 OF indication contacts

or 8 EF combined connected/closed position auxiliary contacts

Optional

OF1–OF4

4 OF indication contacts

Standard

CT1–CT3

CD4–CD6

CE7–CE9

3 CT test position contacts

or 3 CD disconnected position contacts

or 3 CE connected position contacts

Optional

D (with EIFE interface)

OF11–OF22

EF11–EF22

6 OF indication contacts

or 6 EF combined connected/closed position auxiliary contacts

Optional

OF1–OF4

4 OF indication contacts

Standard

EIFE

EIFE embedded Ethernet interface

Optional

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?