DOCA0285EN-04

MasterPacT MTZ2/MTZ3 Range

@TW: this topic is profiled for sharing between MTZ1 with MicAct User Guide and MTZ2/MTZ3 with MicAct User Guide

The MasterPacT MTZ2/MTZ3 range of circuit breakers is made of:

MasterPacT MTZ2/MTZ3 Circuit Breakers with MicroLogic Active Control Unit

The range of MasterPacT MTZ2/MTZ3 circuit breakers with MicroLogic Active control unit offers current ratings from 800 A to 6,300 A for AC power systems up to 690 Vac.

NOTE: For AC power systems with IT grounding system, the voltage is limited to 600 Vac.

MasterPacT MTZ2/MTZ3 circuit breakers with MicroLogic Active control unit are available:

  • In the following frame sizes:

    • MasterPacT MTZ2 for current ratings from 800 A to 4,000 A

    • MasterPacT MTZ3 for current ratings from 4,000 A to 6,300 A

  • In the following power systems:

    • 3-pole (3P)

    • 4-pole (4P)

  • In the following installation types:

    • Fixed-mounted circuit breakers

    • Drawout circuit breakers

Circuit Breakers

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Do not install a MicroLogic Active control unit with version number 004.000.000 in a MasterPacT MTZ circuit breaker with performance level L1 or H3.
Failure to follow these instructions will result in death or serious injury.

MasterPacT MTZ2/MTZ3 circuit breakers with MicroLogic Active control unit are available with the following performance levels:

  • H1: high short-circuit level (66 kA) with total selectivity

  • H2: very high short-circuit level (100 kA) with very high selectivity (85 kA)

Additionally, for MasterPacT MTZ2 circuit breakers with MicroLogic Active control unit:

  • N1: standard short-circuit level (42 kA) with total selectivity

  • H3: extremely high short-circuit level (150 kA) with high selectivity (66 kA)

  • L1: extremely high short-circuit level (150 kA) with strong current limitation and significant selectivity (30 kA)

NOTE: The values above correspond to a 440 Vac network, for higher voltage levels the values can be different. Refer to LVPED225010EN MasterPacT MTZ with MicroLogic Active Control Unit - Catalog.

For full information about available circuit breaker models, interrupting ratings, sensor ratings, and control units, refer to LVPED225010EN MasterPacT MTZ with MicroLogic Active Control Unit - Catalog.

Circuit breakers are fitted with a MicroLogic Active control unit.

For full information about MicroLogic Active control unit, refer to DOCA0265•• MasterPacT MTZ - MicroLogic Active Control Unit - User Guide.

Neutral Position on 4P Circuit Breakers

On 4P circuit breakers:

  • For MasterPacT MTZ2 N1, the neutral position is on the left side as standard.

  • For MasterPacT MTZ2 H1 and H2, the neutral position is on the left side as standard. A version with neutral position on the right side is available when ordering.

  • For MasterPacT MTZ3 H1 and H2, the neutral position is on the left side as standard. A version with neutral position on the right side is available when ordering.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?