DOCA0256EN-01

Analog Module Data

The table lists the analog module data for the PROFIBUS DP communication.

Slot

Index

Byte offset

Size (in bytes)

RW

X

Unit

Type

Svd

Parameter name

1 3

170

2

R

0.1

mA

INT16

N

Analog input 1

1 3

172

2

R

0.1

mA

INT16

N

Analog input 2

1 3

174

2

R

0.1

mA

INT16

N

Analog input 3

1 3

176

2

R

0.1

mA

INT16

N

Analog input 4

1 3

178

8

Reserved

1 3

186

2

R

0.1

mA

INT16

N

Analog output 1

1 3

188

2

R

0.1

mA

INT16

N

Analog output 2

1 3 190 4

Reserved
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.