DOCA0256EN-01

Last Motor Start Time Stamp

The table lists the last motor start time stamp data for the PROFIBUS DP communication.

Slot

Index

Byte offset

Size (in bytes)

RW

X

Unit

Type

Svd

Parameter name

1 3

156

2

R

1

UINT16

Y

Day

1 3

158

2

R

1

UINT16

Y

Month

1 3

160

2

R

1

UINT16

Y

Year

1 3

162

2

R

1

h

UINT16

Y

Hour

1 3

164

2

R

1

min

UINT16

Y

Minute

1 3

166

2

R

1

s

UINT16

Y

Second

1 3

168

2

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.