DOCA0256EN-01

Maximum Number of Starts

The table lists the maximum number of starts data for the PROFIBUS DP communication.

Slot Index

Byte offset

Size (in bytes)

RW

X

Unit

Type

Range

Default value

Svd

Parameter name

1 7

32

2

RW

1

UINT16

  • 0: Disable

  • 1: Enable

1

Y

Function setting

1 7

34

2

RW

1

UINT16

1–30
(step 1)

6

Y

Permissive starts

1 7

36

2

RW

1

min

UINT16

15–60
(step 1)

30

Y

Reference time

1 7

38

2

RW

1

min

UINT16

1–120
(step 1)

5

Y

Inhibit period

1 7

40

2

RW

1

min

UINT16

0–120
(step 1)

0

Y

Time between starts

1 7

42

6

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.