DOCA0256EN-01

Statistic Data

The table lists the statistic data for the PROFIBUS DP communication.

Index

Slot

Byte offset

Size (in bytes)

RW

X

Unit

Type

Svd

Parameter name

1 4

0

2

R

1

ms

UINT16

N

Timer 1 - Actual value

1 4

2

2

R

1

ms

UINT16

N

Timer 2 - Actual value

1 4

4

2

R

1

ms

UINT16

N

Timer 3 - Actual value

1 4

6

2

R

1

ms

UINT16

N

Timer 4 - Actual value

1 4

8

2

R

1

UINT16

N

Counter 1 - Actual value

1 4

10

2

R

1

UINT16

N

Counter 2 - Actual value

1 4

12

2

R

1

UINT16

N

Counter 3 - Actual value

1 4

14

2

R

1

UINT16

N

Counter 4 - Actual value

1 4

16

2

R

1

UINT16

N

Thermal overload trip counter

1 4

18

2

R

1

UINT16

N

Locked rotor trip counter

1 4

20

2

R

1

UINT16

N

Stalled rotor trip counter

1 4

22

2

R

1

UINT16

N

Definite time overcurrent trip counter

1 4

24

2

R

1

UINT16

N

Normal inverse overcurrent trip counter

1 4

26

2

R

1

UINT16

N

Short time overcurrent trip counter

1 4

28

2

R

1

UINT16

N

Calculated ground trip counter

1 4

30

2

R

1

UINT16

N

Measured ground trip counter

1 4

32

2

R

1

UINT16

N

Phase under current trip counter

1 4

34

2

R

1

UINT16

N

Current imbalance trip counter

1 4

36

2

R

1

UINT16

N

Current phase loss trip counter

1 4

38

2

R

1

UINT16

N

Current phase reversal trip counter

1 4

40

2

R

1

UINT16

N

Phase under voltage trip counter

1 4

42

2

R

1

UINT16

N

Phase over voltage trip counter

1 4

44

2

R

1

UINT16

N

Voltage phase loss trip counter

1 4

46

2

R

1

UINT16

N

Voltage imbalance trip counter

1 4

48

2

R

1

UINT16

N

Voltage phase reversal trip counter

1 4

50

2

R

1

UINT16

N

Under frequency trip counter

1 4

52

2

R

1

UINT16

N

Over frequency trip counter

1 4

54

2

R

1

UINT16

N

Excessive start time trip counter

1 4

56

2

R

1

UINT16

N

Communication loss trip counter

1 4

58

2

R

1

UINT16

N

LTMT main unit temperature trip counter

1 4

60

2

R

1

UINT16

N

Under power trip counter

1 4

62

2

R

1

UINT16

N

Over power trip counter

1 4

64

2

R

1

UINT16

N

Under power factor trip counter

1 4

66–78

14

Reserved

1 4

80

2

R

1

UINT16

N

DI interlock 1 trip counter

1 4

82

2

R

1

UINT16

N

DI interlock 2 trip counter

1 4

84

2

R

1

UINT16

N

DI interlock 3 trip counter

1 4

86

2

R

1

UINT16

N

DI interlock 4 trip counter

1 4

88

2

R

1

UINT16

N

DI interlock 5 trip counter

1 4

90

2

R

1

UINT16

N

DI interlock 6 trip counter

1 4

92

2

R

1

UINT16

N

DI interlock 7 trip counter

1 4

94

2

R

1

UINT16

N

DI interlock 8 trip counter

1 4

96

2

R

1

UINT16

N

DI interlock 9 trip counter

1 4

98

2

R

1

UINT16

N

DI interlock 10 trip counter

1 4

100

2

R

1

UINT16

N

DI interlock 11 trip counter

1 4

102

2

R

1

UINT16

N

DI interlock 12 trip counter

1 4

104–150

8

Reserved

1 4

152

2

R

1

UINT16

N

Calculator output 1

1 4

154

2

R

1

UINT16

N

Calculator output 2

1 4

156

2

R

1

UINT16

N

Motor stop error detection trip counter

1 4

158

2

R

1

UINT16

N

Logic test interrupted trip counter

1 4

160

2

R

1

UINT16

N

Stucked reset key trip counter

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.