DOCA0256EN-01

Voltage Dip

The table lists the voltage dip data for the PROFIBUS DP communication.

Slot Index

Byte offset

Size (in bytes)

RW

X

Unit

Type

Range

Default value

Svd

Parameter name

1 7

14

2

RW

1

UINT16

  • 0: Disable

  • 1: Load shedding
  • 2: Auto restart

0

Y

Function setting

1 7

16

2

RW

1

%Vn

UINT16

20–90
(step 5)

90

Y

Voltage dip

1 7

18

2

RW

1

%Vn

UINT16

20–95
(step 5)

95

Y

Voltage restoration

1 7

20

2

RW

1

s

UINT16

0–9999
(step 1)

2

Y

Voltage dip restart timeout

1 7

22

2

RW

1

s

UINT16

0–301
(step 1)

4

Y

Delayed restart timeout

1 7

24

2

RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

Y

Bypass STOP DI

1 7

26

2

RW

1

s

UINT16

0–4
(step 1)

2

Y

Immediate restart timeout

1 7

28

2

RW

1

s

UINT16

1–9999
(step 1)

10

Y

Load shedding timeout

1 7

30

2

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.