DOCA0256EN-01

Locked Rotor Protection

The table lists the locked rotor protection data for the PROFIBUS DP communication.

Slot Index

Byte offset

Size (in bytes)

RW

X

Unit

Type

Range

Default value

Svd

Parameter name

1 5

48

2

RW

1

UINT16

  • 0: Disable

  • 1: Alarm

  • 2: Trip

  • 3: Alarm and Trip

2

Y

Function setting

1 5

50

2

RW

1

%IFLC*

UINT16

150–1000
(step 1)

200

Y

Pickup

1 5

52

2

RW

0.1

s

UINT16

1–60000
(step 1)

100

Y

Time delay

1 5

54

2

RW

1

%IFLC*

UINT16

150–1000
(step 1)

200

Y

Alarm level

1 5

56

2

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI

  • Bit 2: Communication

  • Bit 3: Auto

3

Y

Reset mode

1 5

58

2

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto–Reset delay

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.