DOCA0256EN-01

PROFIBUS DP Settings

The table lists the PROFIBUS DP settings for the PROFIBUS DP communication.

Slot Index

Byte offset

Size (in bytes)

RW

X

Unit

Type

Range

Default value

Svd

Parameter name

1 9

60

2

RW

1

UINT16

2–126
(step 1)

126

Y

Node address

1 9

62

2

RW

1

UINT16

0–1
(step 1)

0

Y

Endian
1 9

64

2

RW

1

UINT16

  • 0: Default

  • 1: TeSys T

  • 2: Other

0

Y

Product profile
1 9

66

6

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.