DOCA0256EN-01

Date and time Settings

The table lists the Date and time settings for the PROFIBUS DP communication.

NOTE: The clock can remembers the date and time for 12 hours without power.

Slot Index

Byte offset

Size (in bytes)

RW

X

Unit

Type

Range

Default value

Svd

Parameter name

1 9

72

2

RW

1

UINT16

1–31
(step 1)

1

Y

Date

1 9

74

2

RW

1

UINT16

1–12
(step 1)

1

Y

Month

1 9

76

2

RW

1

UINT16

2000–2099
(step 1)

2016

Y

Year

1 9

78

2

RW

1

UINT16

0–23
(step 1)

0

Y

Hour

1 9

80

2

RW

1

UINT16

0–59
(step 1)

0

Y

Minute

1 9

82

2

RW

1

UINT16

0–59
(step 1)

0

Y

Second

1 9

84

4

Reserved

1 9

88

2

RW

1

UINT16

0–1
(step 1)

0

N

Update RTC

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.