DOCA0256EN-01

Definite Time Overcurrent Protection

The table lists the definite time overcurrent protection data for the PROFIBUS DP communication.

Slot Index

Byte offset

Size (in bytes)

RW

X

Unit

Type

Range

Default value

Svd

Parameter name

1 5

60

2

RW

1

UINT16

  • 0: Disable

  • 1: Alarm
  • 2: Trip
  • 3: Alarm and Trip

2

Y

Function setting

1 5

62

2

RW

1

%IFLC*

UINT16

20–1000
(step 1)

110

Y

Pickup

1 5

64

2

RW

0.1

s

UINT16

1–60000
(step 1)

300

Y

Time delay during motor start (TpS)

1 5

66

2

RW

0.1

s

UINT16

1–60000
(step 1)

200

Y

Time delay during motor run (TpR)

1 5

68

2

RW

1

%Pickup

UINT16

20–1000
(step 1)

110

Y

Alarm level

1 5

70

2

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI

  • Bit 2: Communication

  • Bit 3: Auto

3

Y

Reset mode

1 5

72

2

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

1 5

74

2

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.