DOCA0256EN-01

System Settings

The table lists the system settings for the PROFIBUS DP communication.

Slot Index

Byte offset

Size
(in bytes)

RW

X

Unit

Type

Range

Default value

Svd

Parameter name

1 9

154

2

RW

1

A

UINT16

1–1000
(step 1)

1

Y

Phase CT primary

1 9

156

2

RW

1

A

UINT16

1–5
(step 4)

1

Y

Phase CT secondary

1 9 158 4 Reserved
1 9

162

2

RW

1

A

UINT16

1–1000
(step 1)

1

Y

Speed 2 CT primary

1 9

164

2

RW

1

A

UINT16

1–5
(step 4)

1

Y

Speed 2 CT secondary

1 9 166 6 Reserved
1 9

172

2

RW

0.1

V

UINT16

1100–6900
(step 1)

4150

Y

Nominal Voltage

1 9

174

2

RW

1

UINT16

  • 0: 50 Hz

  • 1: 60 Hz

0

Y

Nominal frequency

1 9

176

2

RW

1

UINT16

  • 0: L123

  • 1: L132

0

Y

Phase rotation

1 9

178

2

RW

1

UINT16

  • 0: Disable

  • 1: Enable

1

Y

Voltage input**

1 9

180

2

Reserved

1 9

182

2

RW

0.1

A

UINT16

1–10000
(step 1)

25

Y

 Full load current

1 9

184

2

RW

0.1

A

UINT16

1–10000
(step 1)

25

Y

Speed 2 full load current

1 9

186

2

RW

1

UINT16

1–10
(step 1)

1

N Phase CT secondary passes
1 9

188

2

RW

1

UINT16

1–10
(step 1)

1

N Speed 2 phase secondary passes
1 9

190

6

Reserved

1 9

196

2

RW

1

UINT16

  • 0: Disable

  • 1: Enable

1

Y

Test mode

1 9 198

2

RW

1

UINT16

  • 0: No

  • 1: Yes

0

Y

Bypass interlocks during test

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.