DOCA0256EN-01

Device Internal Status

The table lists the device internal status for the PROFIBUS DP communication.

Slot Index

Byte offset

Size (in bytes)

RW

X

Unit

Type

Range

Default value

Svd

Parameter name

1 7

58

2

RW

0.1

s

UINT16

1–60000
(step 1)

10

Y

Time delay

1 7

59

2

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI

  • Bit 2: Communication

  • Bit 3: Auto

3

Y

Reset mode

1 7

60

2

RW

UINT16

  • 0 - Disable

  • 1 - Enable
1 N

Internal temperature alarm

1 7

61

2

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.