DOCA0256EN-01

Stalled Rotor Protection

The table lists the stalled rotor protection data for the PROFIBUS DP communication.

Slot Index

Byte offset

Size (in bytes)

RW

X

Unit

Type

Range

Default value

Svd

Parameter name

1 5

36

2

RW

1

UINT16

  • 0: Disable

  • 1: Alarm

  • 2: Trip

  • 3: Alarm and Trip

2

Y

Function

setting
1 5

38

2

RW

1

%IFLC*

UINT16

50–1000
(step 1)

200

Y

Pickup 

1 5

40

2

RW

0.1

s

UINT16

1–60000
(step 1)

20

Y

Time delay

1 5

42

2

RW

1

%IFLC*

UINT16

50–1000
(step 1)

200

Y

Alarm level

1 5

44

2

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI

  • Bit 2: Communication

  • Bit 3: Auto

3

Y

Reset mode

1 5

46

2

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset Delay

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.