DUG_Adapter_LK-01

Creating a schedule

The Plug can be controlled and triggered by a schedule. Once the schedule is set, your system will follow the active schedule. You can create or modify the schedules at any time.
To create a schedule:
  1. On the Home page, tap All devices > Adapter.
  2. Tap Schedule > Add schedule to add a schedule.
  3. Set the time (A).
  4. Tap Repeat (B) to select the days you want to set the schedule.
  5. Tap Note (C), enter the note and tap Confirm.
  6. Tap the toggle switch (D) to turn on the Notification for the schedule. The app will send a notification that the scheduled task is executed at the time of schedule.
  7. Tap Switch (E) and select one of the options:
    • On - Turns on the Plug at the scheduled time
    • Off - Turns off the Plug at the scheduled time

  8. Tap Save.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?