DUG_Adapter_LK-01

Setting the one-time timer

The One-Time Timer toggles the existing status of the Plug after the selected timer duration is over. Using the Wiser app, you can set the temporary timer to turn on/off the Plug.
To set the timer:
  1. On the Home page, tap All devices > Adapter.
  2. Tap to display set period.
  3. In the slide-up menu, select the Set Period (A) and tap Confirm.
    NOTE:
    • The Customized Period option allows you to set the timer duration for up to 5 hours.

    • The countdown of the timer is updated every 30 seconds.

    • If the Permanent Timer is turned on, then the One-Time Timer is disabled.

  4. To turn off the timer before the timer duration is over, tap .

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?