DUG_Adapter_LK-01

Editing a moment

To edit a moment:
  1. On the Moment tab, locate the moment you want to edit and tap .
  2. On the Edit page, you can tap each item (such as dimmer, shutter, delay, temperature, etc.) to change the settings.
    TIP:
    • You can add one or more actions using .

    • To delete an existing action, slide the each item towards left and tap Delete.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?