DUG_Adapter_LK-01

Removing the device

Using the Wiser app, you can remove a device from the device list.
To remove the device:
  1. On the Home page, tap All devices > Adapter.
  2. Tap to display more details.
  3. Tap Remove Device (A) and select one of the following:
    • Disconnect - The device is disconnected from Wi-Fi
    • Disconnect & Erase Data - The device is disconnected from Wi-Fi and erases the app data

    TIP: On the Home page tap and hold Adapter to remove the device.
    NOTE: By removing the device, you will reset the device. If you still have a problem with the reset, then refer to reset the device manually.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?