DUG_Adapter_LK-01

LED Indications

Pairing

User Action

LED Indication

Status

Press the operation button 3 times within 2 seconds, refer to Pairing.

LED blinks red, once per second.

Pairing mode is active for 180 seconds. When pairing is completed, LED glows red if the operation button is turned On before you start pairing, else the LED turns Off.

Resetting

User Action

LED Indication

Status

Press the operation button 3 times within 2 seconds and hold it down once for > 10 s.

After 10 s, the LED starts blinking red.

The device is in reset mode. It is reset to the factory settings after 10 seconds. The device then restarts and the LED blinks red indicating pairing mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?