DUG_Adapter_LK-01

Managing Plug settings

Using the Wiser app, you can manage various settings of the Plug.

To access the plug settings:

  1. On the Home page, tap All devices > Adapter.

  2. On the device control panel page, tap Settings.

Permanent timer

When the Plug is switched on, the permanent timer turns it off after the selected timer duration is over until the setting is disabled. When the permanent timer is on, the One-Time Timer on the device control panel page is disabled.

To turn on the permanent timer:

  1. Tap the toggle switch (A) to turn on the Permanent Timer.

    This opens the Permanent Timer Duration option.

  2. Tap Permanent Timer Duration (B), select the timer duration and tap Confirm.

    NOTE: The Customized Period option allows you to set the timer duration for up to 5 hours.

EXAMPLE: If you select the timer duration as one minute, then the Plug automatically turns off after one minute.

Power outage status

When power is restored after a power outage, the power outage status setting determines the status of the Plug regardless of the previous status.

Tap Power Outage Status (C) and select one of the following:

Off - If the Plug is turned on before the power outage, then the Plug will be in off status when the power is restored

On - If the Plug is turned off before the power outage, then the Plug will be in on status when the power is restored

Remember last status - The previous status of the device continues

NOTE: The status 5 seconds before the power outage is remembered.

EXAMPLE: If the Plug is in on status 2 seconds before the power outage and in off status 5 seconds before power outage, then the Plug will be in off status when the power is restored.

Child lock

The child lock helps to prevent children from operating the Plug. When the child lock is on, the Plug can be operated only using the app, the operation button on the Plug is disabled.

TIP: By turning on the child lock, the Plug does not turn off, it remains in its current state.

Activate/Deactivate using app

Tap the toggle switch (D) to turn on/off the Child Lock.

Deactivate manually

Short press the operation button four times (< 5 s).

NOTE: If the child lock function is deactivated manually, then the toggle switch (D) in the app displays off status.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?