DUG_Adapter_LK-01

Switching On/Off the device manually

You can switch on/off the Plug manually. The Plug will provide power to the electrical appliance connected to it.
Short press the operation button on the device once to switch On/Off the Plug.

The red LED indicates the On status of the Plug.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?