DUG_Adapter_LK-01

Technical Data

Nominal voltage

230 V AC, 50/60 Hz

Nominal power

Load type Load name Load value

LED

100 W

Incandescent lamp

2300 W

Halogen lamp

2300 W

Motor

600 VA

Iron core transformer

500 VA

Electronic step-down converter

500 VA

Nominal current

10 A

Over-voltage protection

Yes

Over-current protection

Yes

Power consumption

≤ 1 W (relay is ON)

≤ 0.5 W (relay is OFF)

Ambient temperature

+5 °C to +35 °C

Storage temperature

–20 °C to +50 °C

Relative humidity

Max. 95% non-condensing

Neutral conductor

Not required

IP rating

IP20

Communication interface

Wi-Fi®: 2.4 GHz, IEEE802.11 b/g/n

Operating frequency

2.412 GHz to 2.472 GHz

Max. radio-frequency power transmitted

< 40 mW

Range

40 m (indoor line-of-sight)

100 m (outdoor line-of-sight)

Product dimensions

(H X W X D)

61 X 61 X 65 mm

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?