DUG_Adapter_LK-01

Switching On/Off the device using app

Using the Wiser app, you can switch on/off the Plug.
To switch the Plug on/off:
  1. On the Home page, tap the power button (A) to switch on/off the device.

  2. Alternatively, you can navigate to the control panel of the device and tap to switch on/off the Plug.
    NOTE: The control panel shows the current state of the Plug.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?