DUG_Adapter_LK-01

Resetting the device

You can reset the device to factory default manually.
To reset the device:
  1. Short press the operation button 3 times within 2 seconds and then long press the operation button once (>10 s).
  2. After 10 s, LED starts blinking red then release the operation button.
    The LED stops blinking upon successful reset of the device.
  3. The Plug restarts and starts to blink red indicating the pairing mode.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?