For your safety
WARNING |
|---|
|
HAZARD OF UNINTENDED USE
The device is intended to be used for non-critical automation
activities. It is not intended to support life, safety, or medical
equipment.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
CAUTION |
|---|
|
RISK OF DAMAGE TO DEVICE
• The plug must be used indoors only.
• Do not connect any devices that depend on a permanent
power supply.
• Do not mix different load types in the controlled
socket.
• Do not use multi-sockets in the controlled socket.
• Do not use for EV charging.
• To disconnect the plug from the power supply,
pull it out of the socket outlet or turn Off the fuse in the incoming
circuit.
• Do not connect plugs one after another.
Failure to follow these instructions can result in injury or equipment damage.
|
WARNING
CAUTION