DUG_Adapter_LK-01

Pairing the device

Using the Wiser app, pair your device with the local Wi-Fi network to control the device remotely

Before you pair the device, download the Wiser app to your mobile device.

To pair the device:
  1. On the Home page, tap + and tap .
  2. Select the Wi-Fi network, enter the Password (A) and tap Next.
    NOTE: Help to ensure to first connect your mobile phone to the home Wi-Fi and select 2.4 GHz network.

  3. Insert the Plug to a power supply to turnon the device.
  4. Short press the operation button 3 times within 2 seconds on the device regardless of whether it is on or off.
    Help to ensure that the LED blinks red.

  5. In the Wiser app, select Confirm the LED is blinking RED and tap Start Configuration (B) .

    The app displays the progress of connecting the device.

  6. Wait for a few seconds until the device is connected and the app shows that the device is added successfully.
    The red LED on the Plug shows that it is successfully connected to the Wi-Fi network and ready to use.
    NOTE:
    • If the operation button is on before you start pairing, then the LED will glow red when the pairing is complete.

    • If the operation button is off before you start pairing, then the LED will turn Off when the pairing is complete.

  7. Once the device is connected, tap Done.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?