DUG_Adapter_LK-01

Maintenance

It is recommended to clean the device with soft, clean and dry cloth.


NOTICE
Damage to the Device
Do not use cleaning agents to clean the device, as it may damage the device.
Failure to follow these instructions can result in equipment damage.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?