DUG_PowerTagE_WSE-04

Installing the device

It is recommended to install the PowerTag within 3 meters of the Wiser Gateway/Hub for best results. This provides a good network signal strength and helps to prevent online/offline issues, which might result in corrupting data. The signal quality is best maintained when there are no big obstructions (for example thick walls, metal cabinets, etc.) between the PowerTag & Wiser Gateway/Hub. Refer to the installation instruction supplied with this product.

Instruction manual links:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?