DUG_PowerTagE_WSE-04

Setting contract options

You can update flat and peak rate based on your contract option in the Wiser app.
  1. Tap My Contract Options on Electricity page.
  2. In the slide-up menu, select any one of the following (A):
    • Time of Use (Peak/Off-Peak Hours): rate set to a specific period of time at which consumption is at its highest. It is the amount you pay for each unit of electricity consumed for the time period set.
    • Flat Rate: fixed rate for the entire time period of electricity consumption.
    • Spot Price Rate: standard hourly rate of electricity consumption as per tariff zone (for Sweden & Finland).
    • No Contract: electricity rate is not set, no information related to bill will be shown in the app.
    Country without Spotprice (Spain & Portugal) Country with Spotprice (Sweden & Finland)
    NOTE: By default, No Contract option is set.
  3. After selecting an option, tap Confirm.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?