DUG_PowerTagE_WSE-04

Creating an automation

An automation allows you to group multiple actions that are usually done together, triggered automatically or at scheduled times. By using the Wiser app , you can create automations based on your needs.
NOTE: Automation is only possible with the PowerTag assigned as Grid.
  1. On the Home page, tap on .
  2. Go to Automation > + to create an automation.
  3. Tap Edit Name , enter the name of the automation (A) and tap Save.
    TIP: You can choose the cover image that represents your automation by tapping .

  4. Tap Any condition is met to select any one of the condition type (B):
    • All conditions are met: the automation is triggered when all the conditions are met.
    • Any condition is met: the automation is triggered when at least one condition is met.

  5. Tap Add Condition to display the slide-up menu.
  6. In the Add Condition menu, you can do either or all of the following options (C):
    • When weather changes: select various weather settings.
    • Schedule: set the time and day.
    • When device status changes: select the device and its function.
    • When Spot Price Changes: set the spot price and its condition (for Sweden & Finland).
    NOTE: You can add one or more conditions using .

    Country without Spotprice (Spain & Portugal) Country with Spotprice (Sweden & Finland)

  7. Tap When device status changes > Grid and select any of the following function (D):
    • Total Active Power: to set the real-time energy consumption (kW).
    • Load Status: to turn on/off the load.
    • Daily Consumption: to set the daily energy consumption.
    • Monthly Consumption: to set the monthly energy consumption.
  8. For Sweden & Finland, tap When Spot Price Changes, set the required spot price and condition (lesser then/greater then).
    Example: If you set condition as Spot Price > 2 kr/kWh, your actions (defined in next step) will run when price goes above 2 kr/kWh.
  9. Tap Add task to display the slide-up menu.
  10. In the Add task menu, you can do either or all of the following options (E):
    • Run the device: select the devices that you want to trigger.
    • Moment or Automation: select the moment which you want to trigger or select the automation that you want to enable or disable.
    • Send notification: turn on notification for the automation.
    • Delay: set the delay time.
    NOTE: You can add one or more actions using .

  11. Tap on Effective period to set the time range for the automation. You can select any one of the following (F):
    • All-day: 24 hours
    • Daytime: From sunrise to sunset
    • Night: From sunset to sunrise
    • Custom: User defined time period

  12. Once all the actions and conditions are set, tap Save.
    Once the automation is saved, it is visible on the Automation tab. You can tap the toggle switch to enable/disable.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?