DUG_PowerTagE_WSE-04

Personalized Energy Insights

NOTE: Personalized Energy Insights is available only in Sweden & Finland.

Personalized Energy Insights is an energy management feature dedicated to monitor the way we use energy in our everyday life. This feature estimates energy consumption of a household purely based on data from their utility.

This makes it possible to follow the consumed energy over time and calculate a load/energy consumption and provides you with the following personalized energy insights:

  • comparison of energy consumption with similar homes

  • breakdown of energy consumption

  • energy saving tips

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?