DUG_PowerTagE_WSE-04

Creating/updating home profile

User must create a home profile to compare the energy consumption with similar home profiles and also to get the energy usage breakdown based on categories like heating, cooking, lighting, washing etc.

To create home profile:
  1. On the Home Profile page tap Continue.
  2. Select the type of home and tap Next:
    • House
    • Apartment
    • Semi-detached
    • Holiday Home
    • Other

    NOTE: Based on the type of home step 4 to step 12 may differ.
  3. Set the size of your home either by tapping (A) or using the sliding bar (B).

    NOTE: Maximum home size can be 400 sq m.
  4. Set the number of people living in the home either by tapping (C) or using the sliding bar (D).

    NOTE: Maximum 10 people can be added.
  5. Select the main heating system and tap Next:
    • District Heating
    • Radiators
    • Air/Air Heat Pump
    • Water Pan
    • Rock Heat
    • Exhaust Air Heat Pump
    • Other/Unknown

  6. Select the applicable secondary heating systems and tap Next:
    • Radiators
    • District Heating
    • Air/Air Heat Pump
    • Air Water Heat Pump
    • Water Pan
    • Rock Heat
    • Exhaust Air Heat Pump
    • Floor Heat
    • Other / Unknown

  7. Select the type of hot water system and tap Next:
    • Hot Water Tank
    • Air/Air Heat Pump
    • Air Water Heat Pump
    • Rock Heat
    • District Heating
    • Other / Unknown

  8. Select the appliances used to cook and tap Next:
    • Gas Stoves
    • Gas Ovens
    • Electric Stoves
    • Electric Ovens
    • Microwaves
    NOTE:
    • By default it will be 0, use +/- to set the number.

    • Maximum of 5 individual appliances can be added.

  9. Select the appliances in your home and tap Next:
    • Washing Machines
    • Dishwashers
    • Dryers
    • TVs
    • Game Consoles
    • Laptops
    • Stationary Computers
    NOTE: Maximum 5 individual appliances can be added.

  10. Select the fridges and freezers from the list:
    • Fridge
    • Freezer
    • Fridge and Freezer
    NOTE: Maximum 5 individual appliances can be added.

  11. Select the number of Electric cars, tap Complete and then tap Done.

    NOTE: To update the home profile, on the Home page, tap Energy Dashboard > Insights > Update my home profile, follow from step 2.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?